RT1062 ENC module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1062 ENC module

1,847 Views
lewu1
Contributor I

Dear supporter,
I use RT1062 to realize the ENC function.
Can pin GPIO_SPI_B1_00~GPIO_SPI_B1_07 be configured as the PhaseA or PhaseB input?
If not, can pin GPIO_AD_B0_08~GPIO_AD_B0_11 be configured as the PhaseA or PhaseB input?
Thanks a lot.

Labels (2)
0 Kudos
Reply
3 Replies

1,748 Views
mayliu1
NXP Employee
NXP Employee

Hi @lewu1 ,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

Q1:Can pin GPIO_SPI_B1_00~GPIO_SPI_B1_07 be configured as the PhaseA or PhaseB input?

A1: I double checked pin GPIO_SPI_B1_00~GPIO_SPI_B1_07, and I don't believe these pins can be configured as the PhaseA or PhaseB input.

Q2: If not, can pin GPIO_AD_B0_08~GPIO_AD_B0_11 be configured as the PhaseA or PhaseB input?

A2:  Yes, GPIO_AD_B0_08~GPIO_AD_B0_11  pins can be configured as the PhaseA or PhaseB input.

For your better understanding, I post some figs for you.

Snipaste_2026-03-17_17-09-47.pngSnipaste_2026-03-17_17-09-19.png

 

 

 

Wish it helps you

Best Regards

MayLiu

0 Kudos
Reply

1,591 Views
lewu1
Contributor I

Thank you.

0 Kudos
Reply

1,588 Views
mayliu1
NXP Employee
NXP Employee

You are welcome.

If my post answer your question, please press "Accept as solution".

Best Regards

0 Kudos
Reply