Hi community,
I'm struggeling with the power supply pin configuration of MCXN236VDFT. I want to keep the DCDC disabled, but don't get clarity about the multiple power pins of the microcontroller.
According to the comments in the FRDM-MCXN236 schematics, pins VDD_DCDC and DCDC_LX are pulled to GND through 10kR. But the therein mentioned suggestion is to disconnect VDD_CORE pins from the MCU supply, just keep the capacitors connected. But the datasheet shows that this pin is an input (-> requires an external power source for my understanding). However, somewhere else the datasheet mentions that the LDO_CORE pin is an output ("When the LDO_CORE is bypassed, the input VDD_LDO_CORE and output VOUT_CORE/VDD_CORE should be connected together...")
Which is correct? How should I connect the VOUT_CORE?
Furthermore, why should one byass the LDO_SYS by connecting (suggested option in FRDM schematic)?
Looking forward to you feedback.
Best Regards
Weber