Power Estimation Tool for MPC5777C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power Estimation Tool for MPC5777C

1,034 Views
Gabgoes
Contributor I

Hello, my name is Gabriel.

I would like to know if there is a tool or spreadsheet to estimate electrical power dissipation in processor MPC5777C.

Best Regards,

Gabriel Napoli Goes

Electronics Hardware Engineer.

Labels (1)
0 Kudos
Reply
1 Reply

1,018 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

This device is not primarily targeted for low-power applications so Power estimation tool is not provided. 

The only information we have on current is in the datasheet where we give only the worst-case figures.  We do not have data taken for single core operation or reduced frequency operation.  The worst-case current draw is dominated by leakage current at hot temperature and fast process.  Clock speed does not significantly reduce this number.

As for I/O current, this depends on pad usage in the customer application.  See table 11 in the datasheet, rev 14.

0 Kudos
Reply