PCA9450C for IMX8Plus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA9450C for IMX8Plus

918件の閲覧回数
Sourour
Contributor I

Hello NXP community,

We are using the PMIC @PCA9450CHNY in our project to power on the MPU #IMX8Plus. We intend to use LDO4 to generate a power rail of 2V5 for other components on the board.

We need clarification on whether this is feasible (given that it's OFF by default). Additionally, if we decide to use it, will the sequence be the same as with the PCA9450AA, or do we need to configure it using the I2C Bus?

Furthermore, will the sequence be generated directly by the 5V SYS power, or does it require the I2C control of the IMX8?

Thanks.

 

Sourour_0-1710772079862.png

 

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

888件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

 

I suggest you take a look on next links where LDO4CTRL register value es defined:

 

pca9450.h

 

pca9450-regulator.c

 

Best regards.

0 件の賞賛
返信