One MCLK for two SAI-Interfaces

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

One MCLK for two SAI-Interfaces

1,099 Views
HelloWorld121
Contributor I

Hello,

I use i.MX8m mini and, and I want to operate two SAI-Interfaces at the same time.  

It is possible to use a single MCLK for two SAI-interfaces (e.g. SAI5 and SAI6)????

If yes, are there any Disadvantages ??

 

Labels (1)
0 Kudos
Reply
1 Reply

1,078 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

The transmitter and receiver can independently select between the bus clock and up to three audio master clocks to generate the bit clock. The \consideration is if you use a shared MCLK signal for your SAI ports, SAI5 or SAI6 should be configured in Synchronous mode between ports.

Best regards.

0 Kudos
Reply