One MCLK for two SAI-Interfaces

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

One MCLK for two SAI-Interfaces

1,042件の閲覧回数
HelloWorld121
Contributor I

Hello,

I use i.MX8m mini and, and I want to operate two SAI-Interfaces at the same time.  

It is possible to use a single MCLK for two SAI-interfaces (e.g. SAI5 and SAI6)????

If yes, are there any Disadvantages ??

 

ラベル(1)
0 件の賞賛
返信
1 返信

1,021件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

The transmitter and receiver can independently select between the bus clock and up to three audio master clocks to generate the bit clock. The \consideration is if you use a shared MCLK signal for your SAI ports, SAI5 or SAI6 should be configured in Synchronous mode between ports.

Best regards.

0 件の賞賛
返信