NBU functions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NBU functions

1,378 Views
Chan_17
Contributor III

Hello NXP team,
I am using bare KW45 bare MCU and for enabling Radio core for flashing NBU image and Cm33 image I referred AN14003 Rev. 1.1 but I have some queries with respect to function mentioned in the document .
1.Function JiaTest_Set_LifeCycleAndKeys_Secure  use program the fuse but in the definition of the function there is no reference present for the specific variable which is &TestContextForWriteLC , how to succesfully build the project if reference is not present and why reference is not present for the specific variable.
2. I have noticed there is no #if defined in specific part but # endif is present.
NOTE you can find reference of the function in page number 11 and 12 of the document

Labels (2)
0 Kudos
Reply
2 Replies

1,345 Views
luis_maravilla
NXP Employee
NXP Employee

Hello,

The initialization for the context is shown in figure 9 chapter 5.2.1 before the SB3KDK and RoTKTH keys.

You can enter context name: nboot_context_t TestContextForWriteLC; for example.

This is something every customer would need to implement by their side with his own context name.

Best Regards

Luis

0 Kudos
Reply

1,373 Views
Chan_17
Contributor III

attached screenshots unnamed.pngimage (13).png

Tags (1)
0 Kudos
Reply