Hello @Gayathriii ,
Thanks for your post. You may find some helpful tips in Vision ML with the FRDM-MCXN947, which could be useful for addressing this issue.
1. After POR there may be some glitching on the camera due to the fact the camera is expecting 2.8V but the board is at 3.3V and the initial HSYNC signal was missed. Press the reset button (SW1) and it should fix any camera issue.
2. Please confirm the OV7670 camera is plugged into J11 (not J9) and the LCD-PAR-S035 is connected to J12

3. Confirm correct solder jumper orientation for SJ16, SJ26, and SJ27
Hope it helps. Please let me know if you still have problem on this.
BR
Celeste