MCXN947 EVK cannot initialize PHY

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCXN947 EVK cannot initialize PHY

Jump to solution
372 Views
embedbytes
Contributor III

I am starting a new project using the MCXN947. I have both the FRDM-MCXN947 and the MCX-N9XX-EVK demo boards. I will be utilizing LWIP so I downloaded the LWIP-PING examples for both boards. The example runs fine on the FRDM but will not run on the EVK. I keep getting "Cannot initialize PHY" on the EVK. Both boards seem to have the same PHY chip (lan8741A-EN). Can someone offer a little guidance on the issue, it would be much appreciated.

0 Kudos
Reply
1 Solution
321 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @embedbytes,

Are you making sure to follow the board setting that are listed on the "example_board_readme.md" file for the MCX-N9XX-EVK? These include:

Connecting JP13 2-3 pin.
Populating R274 to sync reference clock.

BR,
Edwin.

View solution in original post

0 Kudos
Reply
2 Replies
322 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @embedbytes,

Are you making sure to follow the board setting that are listed on the "example_board_readme.md" file for the MCX-N9XX-EVK? These include:

Connecting JP13 2-3 pin.
Populating R274 to sync reference clock.

BR,
Edwin.

0 Kudos
Reply
137 Views
embedbytes
Contributor III

Yes, Thank for the guidance , all is good now

 

0 Kudos
Reply