MCXN547 thermal simulation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCXN547 thermal simulation

1,742 Views
WJC
Contributor I

Hello,

The customer needs to perform system-level thermal simulation. How can we request the PDML file for MCXN547?

 

Thanks.

WJC

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

1,664 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @WJC , Which package is being requested?

0 Kudos
Reply

1,656 Views
WJC
Contributor I
This is the model MCXN547VPBT, thank you for your assistance in confirming.
0 Kudos
Reply

1,684 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @WJC ,

Thanks for your post. I'm not sure if we have such a file for the MCXN547. Let me confirm it with the internal team.
I'll let you know as soon as I make any progress.

BRs,

Celeste

0 Kudos
Reply

1,566 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @WJC ,

Hope this message finds you well. I'm leaving this note to let you know that I haven't forgotten about your post.

I've checked with the internal team, and they informed me that they are still working on this. Generally, a request of this will takes around two weeks.

I think such a file cannot be released through public channels like the community. I suggest you create a new private case in the following way.

Screenshot 2025-03-20 184052.png

In the case, you can mention me so that I can continue to assist you regarding this case.

Have a nice day!

Celeste

 

----------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
----------------------------------------------------------------------------------------------------------------

0 Kudos
Reply