MCXA153VLF internal clock frequency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCXA153VLF internal clock frequency

跳至解决方案
807 次查看
_Ferrari_
Contributor V

Dear all,

I'm developing a project based on the MCXA153VLF CPU, equipped with an external Crystal Oscillator. I'm using a 16MHz Crystal oscillator. 

I would like to know if he FIRC (fast internal reference clock) can be sincronized with external clock in order to use internal 96MHz clock, generated by FIRC, as main clock.

_Ferrari__2-1750749254181.png

Is it possible to use the "highlighted block" (int the red ellipse) to syncronize FIRC with external clock ? if so, how to do it ?

if not how to syncronize the FIRC with the external clock ?

Thank you very much for your help and cooperation

regards

标签 (2)
0 项奖励
回复
1 解答
767 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @_Ferrari_ 

Yes — the FIRC in the MCXA153 can be auto-trimmed using the external crystal oscillator (SOSC) as a reference clock.

This is supported and described in section 22.6.3.2 "FIRC auto trim example" of the MCXA153 reference Manual.

Harry_Zhang_0-1750907068419.png

BR

Harry

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
768 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @_Ferrari_ 

Yes — the FIRC in the MCXA153 can be auto-trimmed using the external crystal oscillator (SOSC) as a reference clock.

This is supported and described in section 22.6.3.2 "FIRC auto trim example" of the MCXA153 reference Manual.

Harry_Zhang_0-1750907068419.png

BR

Harry

 

0 项奖励
回复