MCXA153VLF internal clock frequency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCXA153VLF internal clock frequency

ソリューションへジャンプ
801件の閲覧回数
_Ferrari_
Contributor V

Dear all,

I'm developing a project based on the MCXA153VLF CPU, equipped with an external Crystal Oscillator. I'm using a 16MHz Crystal oscillator. 

I would like to know if he FIRC (fast internal reference clock) can be sincronized with external clock in order to use internal 96MHz clock, generated by FIRC, as main clock.

_Ferrari__2-1750749254181.png

Is it possible to use the "highlighted block" (int the red ellipse) to syncronize FIRC with external clock ? if so, how to do it ?

if not how to syncronize the FIRC with the external clock ?

Thank you very much for your help and cooperation

regards

ラベル(2)
0 件の賞賛
返信
1 解決策
761件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @_Ferrari_ 

Yes — the FIRC in the MCXA153 can be auto-trimmed using the external crystal oscillator (SOSC) as a reference clock.

This is supported and described in section 22.6.3.2 "FIRC auto trim example" of the MCXA153 reference Manual.

Harry_Zhang_0-1750907068419.png

BR

Harry

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
762件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @_Ferrari_ 

Yes — the FIRC in the MCXA153 can be auto-trimmed using the external crystal oscillator (SOSC) as a reference clock.

This is supported and described in section 22.6.3.2 "FIRC auto trim example" of the MCXA153 reference Manual.

Harry_Zhang_0-1750907068419.png

BR

Harry

 

0 件の賞賛
返信