MCX C SERIES PROGRAMMER

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCX C SERIES PROGRAMMER

1,655件の閲覧回数
RACHIT_JUTHANI
Contributor I

HI I would like to understand if I am using MCX C SERIES then how to program the MCU . What programmer do I have to use? And for MCX N/A/W  do I have to change the programmer or same can be used. I am asking for a mass manufacturing and also for proto testing .

Thank you.

ラベル(4)
0 件の賞賛
返信
1 返信

1,606件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @RACHIT_JUTHANI ,

Thanks for contacting NXP Tech Support. Apologies for the late reply. For mass manufacturing, we more strongly recommend using PEmicro Cyclone programmers/PEmicro Cyclone FX programmer. The page for NXP products they support is as follows: PEmicro Partners . There, you can see all of the MCX A/C/N/W devices. MCX C and W are listed in the wrong category under Kinetis.

Regarding the selection of PEmicro programmers, you can contact PEmicro support. We hope the above information is helpful to you.

Best Regards

Celeste

0 件の賞賛
返信