MCUXpresso Secure Provisioning Tool for MCX C series

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso Secure Provisioning Tool for MCX C series

ソリューションへジャンプ
1,244件の閲覧回数
hermus
Contributor II

In the MCU Xpresso Secure Provisioning Tool V9.0.1 for Windows, I did not see any options for the MCX C series.

Can this tool support the MCXC series MCUs?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,201件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @hermus 

I'm sorry, I misunderstood your previous information. This tool currently does not support the MCXC series.

BR

Hang

元の投稿で解決策を見る

3 返答(返信)
1,217件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @hermus 

This tool support the MCXC series MCUs.

HangZhang_0-1726816368747.png

BR

Hang

0 件の賞賛
返信
1,209件の閲覧回数
hermus
Contributor II
Hi @Harry_Zhang
The chart seems to show support for the MCX N Series and MCX A Series.
Does this mean that selecting any processor from these two series can also support the MCX C04x/14x/24x/44x models?
0 件の賞賛
返信
1,202件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @hermus 

I'm sorry, I misunderstood your previous information. This tool currently does not support the MCXC series.

BR

Hang