MCUExpresso Code Config Tool is not generating driver header file for PWM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUExpresso Code Config Tool is not generating driver header file for PWM

3,763件の閲覧回数
madjapne
Contributor I

Hi,

 

I am using a FRDM-MCXN947 board and trying to configure PWM.

There are two issues, first is some warning related to the Fault line and second it's not generating the "fsl_pwm.h" file.

The "peripheral.h" file was updated to include the "fsl_pwm.h" file and hence the project doesn't compile.

What am I supposed to do?

Thanks,

Rahul

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,719件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @madjapne 

If there are no issues with compilation, you don't need to pay attention to warnings.

If there is no not generating the "fsl_pwm.h" file.

Alternatively, you can try using MCUXpresso IDE, which integrates the config tool and automatically adds missing files.

Hope this will help you.

BR

Hang

0 件の賞賛
返信

3,709件の閲覧回数
madjapne
Contributor I

Hi Hang,

I am using MCUXpresso itself and the building of the project fails because of this error.

Thanks,

Rahul

0 件の賞賛
返信

3,682件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @madjapne 

You can refer to the Video that i uploaded.

Hope this will help you.

BR

Hang

0 件の賞賛
返信