MCPTE1AK116 PMSM FOC sample code error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCPTE1AK116 PMSM FOC sample code error

2,624 Views
Durgaprasad02
Contributor II
 

i imported example from MCSPTE1AK116 but i got error(refer image)when i build project.

508ad121-b615-46e2-810b-214cc8a29458.jpg

 

 #MCPTE1AK116

Labels (1)
0 Kudos
Reply
7 Replies

2,602 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

I must admit that I can't distinguish the text from your image. Please share a new one, preferably with a light theme, which is more distinguishable when sharing IDE screenshots.

Meanwhile, application software MCSPTE1AK116-SW Rev 1.1 works with S32DS for ARM 2.2 and SDK for S32K1xx 3.0.3.

_Leo__0-1742492493831.png

Please make sure you are working with these versions.

Have a nice day!

0 Kudos
Reply

2,589 Views
Durgaprasad02
Contributor II

Hi Leo,

Error  getting ;

Durgaprasad02_0-1742536823776.png

 

Software version:

Durgaprasad02_1-1742536911110.png

 

SDK Package : 

Durgaprasad02_2-1742537004031.png

 

Could please if any Motor control example code for S32k118.

 

thank you!!

0 Kudos
Reply

2,572 Views
_Leo_
NXP TechSupport
NXP TechSupport

Please download the following IDE and update from S32DS-ARM page -> Downloads section, in order to run the MCSPTE1AK116-SW Rev 1.1:

_Leo__0-1742578993543.png

On the other hand, there is no such demo for S32K118, just for S32K116, for migration you just need to consider their differences in Feature comparison section of datasheet.

0 Kudos
Reply

2,536 Views
Durgaprasad02
Contributor II

Hi leo,

I've install S32 Design Arm Version below given error coming. 

Durgaprasad02_0-1742836934441.png

 

0 Kudos
Reply

2,529 Views
_Leo_
NXP TechSupport
NXP TechSupport

GFLIB is included in AMMCLIB. Please, set your library paths accordingly your files location in project settings.

Includes and also libraries paths:

_Leo__0-1742855586425.png_Leo__1-1742855598352.png

 

0 Kudos
Reply

2,501 Views
Durgaprasad02
Contributor II

Hi Leo,

The settings are already as per your suggestion.

0 Kudos
Reply

2,475 Views
_Leo_
NXP TechSupport
NXP TechSupport

I hope it worked. Any other questions feel free to continue using our Technical Support Service.

0 Kudos
Reply