MC33771c TPL communication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC33771c TPL communication

1,261件の閲覧回数
Miral
Contributor I

The communication works correctly with the MC33771B using a specific implementation and BCC library. I can successfully send commands and receive valid response frames.

However, when I use the same communication code and only replace the BCC library/configuration for the MC33771C, I receive only the echo frame and no valid response from the device.

The SPI/TPL timing, frame format, and hardware connections remain the same. The wake-up sequence and INIT sequence are also implemented.

Has anyone experienced this issue with MC33771C?


bcc_status_t BCC_MCU_TransferTpl(uint8_t drvInstance, uint8_t transBuf[], uint8_t recvBuf[], uint16_t recvTrCnt)

{

uint16_t recvSize;

if(recvTrCnt > 0)

recvSize = (recvTrCnt - 1) * 6U;

else recvSize = 6U;

HAL_SPI_DeInit(&hspi2);

HAL_Delay(2);

HAL_SPI_Init(&hspi2);

memset(recvBuf, 0, sizeof(&recvBuf));

HAL_GPIO_WritePin(CS_TX_GPIO_Port, CS_TX_Pin, GPIO_PIN_RESET); HAL_SPI_Receive_IT(&hspi2, recvBuf, 6);

rxflag = 0;

if(HAL_SPI_Transmit_IT(&hspi1, transBuf, 6) != HAL_OK)

{ HAL_GPIO_WritePin(CS_TX_GPIO_Port, CS_TX_Pin, GPIO_PIN_SET);

return BCC_STATUS_PARAM_RANGE;

}

BCC_MCU_WaitUs(5);

if(spi2_rx_done == 1)

{

HAL_SPI_Receive_IT(&hspi2, recvBuf, recvSize);

spi2_rx_done = 0;

}

HAL_GPIO_WritePin(CS_TX_GPIO_Port, CS_TX_Pin, GPIO_PIN_SET);

return BCC_STATUS_SUCCESS;

}

int MC33771_Init(void)

{

HAL_GPIO_WritePin(EN_GPIO_Port, EN_Pin, GPIO_PIN_RESET);

HAL_Delay(1);

HAL_GPIO_WritePin(EN_GPIO_Port, EN_Pin, GPIO_PIN_SET);

HAL_Delay(10);

g_bccConfig.drvInstance = 0;

g_bccConfig.commMode = BCC_MODE_TPL;

g_bccConfig.devicesCnt = 1;

g_bccConfig.device[0] = BCC_DEVICE_MC33771C;

g_bccConfig.cellCnt[0] = 14;

status = BCC_Init(&g_bccConfig);

if(status != BCC_STATUS_SUCCESS)

{

return (int)status;

}

}

void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)

{

if(hspi->Instance == SPI2)

spi2_rx_done = 1;

}

static void MX_SPI1_Init(void)

{

hspi1.Instance = SPI1;

hspi1.Init.Mode = SPI_MODE_MASTER;

hspi1.Init.Direction = SPI_DIRECTION_2LINES;

hspi1.Init.DataSize = SPI_DATASIZE_8BIT;

hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;

hspi1.Init.CLKPhase = SPI_PHASE_2EDGE;

hspi1.Init.NSS = SPI_NSS_SOFT;

hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_8;

hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;

hspi1.Init.TIMode = SPI_TIMODE_DISABLE;

hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;

hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;

if(HAL_SPI_Init(&hspi1) != HAL_OK)

{

Error_Handler();

}

}

static void MX_SPI2_Init(void)

{

hspi2.Instance = SPI2;

hspi2.Init.Mode = SPI_MODE_SLAVE;

hspi2.Init.Direction = SPI_DIRECTION_2LINES_RXONLY;

hspi2.Init.DataSize = SPI_DATASIZE_8BIT;

hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;

hspi2.Init.CLKPhase = SPI_PHASE_2EDGE;

hspi2.Init.NSS = SPI_NSS_HARD_INPUT;

hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;

hspi2.Init.TIMode = SPI_TIMODE_DISABLE;

hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;

hspi2.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;

if(HAL_SPI_Init(&hspi2) != HAL_OK)

{

Error_Handler();

}

}

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,213件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Miral,

I need to contact Software engineer for your issue. Please share following information about your project. They always require the information. 

Customer: AARTRONIX INNOVATIONS

End Customer: ? (can be also AARTRONIX INNOVATIONS)

End Application: ?

Country: India

Annual Volume: ?

With Best Regards,

Jozef

0 件の賞賛
返信

1,209件の閲覧回数
Miral
Contributor I

Customer: AARTRONIX INNOVATIONS

End Customer: AAROHI EMBEDDED SYSTEM PVT LTD 

End Application: UPS Battery backup

Country: India

Annual Volume:1000

0 件の賞賛
返信

1,097件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Miral,

please see below an answer from the application engineer. Please share a scope as requested.

DESCRIPTION

It would really help if the customer could get a scope trace or Saleae output of the transmissions to really see what is going on.  Note that the MC33771B is TPL1 (40-bit) and MC33771C is TPL2 (48-bit).  Also, the customer can reference the MC33771C SDK attached.

With Best Regards,

Jozef

0 件の賞賛
返信
%3CLINGO-SUB%20id%3D%22lingo-sub-2369103%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3EMC33771c%20TPL%E9%80%9A%E4%BF%A1%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2369103%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3E%E7%89%B9%E5%AE%9A%E3%81%AE%E5%AE%9F%E8%A3%85%E3%81%A8BCC%E3%83%A9%E3%82%A4%E3%83%96%E3%83%A9%E3%83%AA%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%99%E3%82%8B%E3%81%93%E3%81%A8%E3%81%A7%E3%80%81MC33771B%E3%81%A8%E3%81%AE%E9%80%9A%E4%BF%A1%E3%81%AF%E6%AD%A3%E5%B8%B8%E3%81%AB%E5%8B%95%E4%BD%9C%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%E3%82%B3%E3%83%9E%E3%83%B3%E3%83%89%E3%81%AE%E9%80%81%E4%BF%A1%E3%81%A8%E6%9C%89%E5%8A%B9%E3%81%AA%E5%BF%9C%E7%AD%94%E3%83%95%E3%83%AC%E3%83%BC%E3%83%A0%E3%81%AE%E5%8F%97%E4%BF%A1%E3%81%AF%E6%AD%A3%E5%B8%B8%E3%81%AB%E8%A1%8C%E3%81%88%E3%81%BE%E3%81%97%E3%81%9F%E3%80%82%3C%2FP%3E%3CP%3E%E3%81%97%E3%81%8B%E3%81%97%E3%80%81%E5%90%8C%E3%81%98%E9%80%9A%E4%BF%A1%E3%82%B3%E3%83%BC%E3%83%89%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%80%81MC33771C%E7%94%A8%E3%81%AEBCC%E3%83%A9%E3%82%A4%E3%83%96%E3%83%A9%E3%83%AA%2F%E8%A8%AD%E5%AE%9A%E3%81%AE%E3%81%BF%E3%82%92%E7%BD%AE%E3%81%8D%E6%8F%9B%E3%81%88%E3%81%9F%E5%A0%B4%E5%90%88%E3%80%81%E3%82%A8%E3%82%B3%E3%83%BC%E3%83%95%E3%83%AC%E3%83%BC%E3%83%A0%E3%81%AE%E3%81%BF%E3%82%92%E5%8F%97%E4%BF%A1%E3%81%97%E3%80%81%E3%83%87%E3%83%90%E3%82%A4%E3%82%B9%E3%81%8B%E3%82%89%E3%81%AE%E6%9C%89%E5%8A%B9%E3%81%AA%E5%BF%9C%E7%AD%94%E3%81%AF%E5%BE%97%E3%82%89%E3%82%8C%E3%81%BE%E3%81%9B%E3%82%93%E3%80%82%3C%2FP%3E%3CP%3ESPI%2FTPL%E3%81%AE%E3%82%BF%E3%82%A4%E3%83%9F%E3%83%B3%E3%82%B0%E3%80%81%E3%83%95%E3%83%AC%E3%83%BC%E3%83%A0%E3%83%95%E3%82%A9%E3%83%BC%E3%83%9E%E3%83%83%E3%83%88%E3%80%81%E3%81%8A%E3%82%88%E3%81%B3%E3%83%8F%E3%83%BC%E3%83%89%E3%82%A6%E3%82%A7%E3%82%A2%E6%8E%A5%E7%B6%9A%E3%81%AF%E5%A4%89%E6%9B%B4%E3%81%82%E3%82%8A%E3%81%BE%E3%81%9B%E3%82%93%E3%80%82%E3%82%A6%E3%82%A7%E3%82%A4%E3%82%AF%E3%82%A2%E3%83%83%E3%83%97%E3%82%B7%E3%83%BC%E3%82%B1%E3%83%B3%E3%82%B9%E3%81%A8INIT%E3%82%B7%E3%83%BC%E3%82%B1%E3%83%B3%E3%82%B9%E3%82%82%E5%AE%9F%E8%A3%85%E3%81%95%E3%82%8C%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3EMC33771C%E3%81%A7%E3%81%93%E3%81%AE%E5%95%8F%E9%A1%8C%E3%81%8C%E7%99%BA%E7%94%9F%E3%81%97%E3%81%9F%E6%96%B9%E3%81%AF%E3%81%84%E3%81%BE%E3%81%99%E3%81%8B%EF%BC%9F%3C%2FP%3E%3CP%3E%3CBR%20%2F%3Ebcc_status_t%20BCC_MCU_TransferTpl(uint8_t%20drvInstance%2C%20uint8_t%20transBuf%5B%5D%2C%20uint8_t%20recvBuf%5B%5D%2C%20uint16_t%20recvTrCnt)%3C%2FP%3E%3CP%3E%7B%3C%2FP%3E%3CP%3Euint16_t%20recvSize%3B%3C%2FP%3E%3CP%3Eif(recvTrCnt%20%26gt%3B%200)%3C%2FP%3E%3CP%3ErecvSize%20%3D%20(recvTrCnt%20-%201)%20*%206U%3B%3C%2FP%3E%3CP%3E%E3%81%9D%E3%82%8C%E4%BB%A5%E5%A4%96%E3%81%AE%E5%A0%B4%E5%90%88%E3%81%AF%E3%80%81recvSize%20%3D%206U%3B%3C%2FP%3E%3CP%3EHAL_SPI_DeInit(%26amp%3Bhspi2)%3B%3C%2FP%3E%3CP%3EHAL_Delay(2)%3B%3C%2FP%3E%3CP%3EHAL_SPI_Init(%26amp%3Bhspi2)%3B%3C%2FP%3E%3CP%3Ememset(recvBuf%2C%200%2C%20sizeof(%26amp%3BrecvBuf))%3B%3C%2FP%3E%3CP%3EHAL_GPIO_WritePin(CS_TX_GPIO_Port%2C%20CS_TX_Pin%2C%20GPIO_PIN_RESET)%3B%20HAL_SPI_Receive_IT(%26amp%3Bhspi2%2C%20recvBuf%2C%206)%3B%3C%2FP%3E%3CP%3Erxflag%20%3D%200%3B%3C%2FP%3E%3CP%3Eif(HAL_SPI_Transmit_IT(%26amp%3Bhspi1%2C%20transBuf%2C%206)%20!%3D%20HAL_OK)%3C%2FP%3E%3CP%3E%7B%20HAL_GPIO_WritePin(CS_TX_GPIO_Port%2C%20CS_TX_Pin%2C%20GPIO_PIN_SET)%3B%3C%2FP%3E%3CP%3EBCC_STATUS_PARAM_RANGE%20%E3%82%92%E8%BF%94%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3E%7D%3C%2FP%3E%3CP%3EBCC_MCU_WaitUs(5)%3B%3C%2FP%3E%3CP%3Eif(spi2_rx_done%20%3D%3D%201)%3C%2FP%3E%3CP%3E%7B%3C%2FP%3E%3CP%3EHAL_SPI_Receive_IT(%26amp%3Bhspi2%2C%20recvBuf%2C%20recvSize)%3B%3C%2FP%3E%3CP%3Espi2_rx_done%20%3D%200%3B%3C%2FP%3E%3CP%3E%7D%3C%2FP%3E%3CP%3EHAL_GPIO_WritePin(CS_TX_GPIO_Port%2C%20CS_TX_Pin%2C%20GPIO_PIN_SET)%3B%3C%2FP%3E%3CP%3EBCC_STATUS_SUCCESS%20%E3%82%92%E8%BF%94%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3E%7D%3C%2FP%3E%3CP%3Eint%20MC33771_Init(void)%3C%2FP%3E%3CP%3E%7B%3C%2FP%3E%3CP%3EHAL_GPIO_WritePin(EN_GPIO_Port%2C%20EN_Pin%2C%20GPIO_PIN_RESET)%3B%3C%2FP%3E%3CP%3EHAL_Delay(1)%3B%3C%2FP%3E%3CP%3EHAL_GPIO_WritePin(EN_GPIO_Port%2C%20EN_Pin%2C%20GPIO_PIN_SET)%3B%3C%2FP%3E%3CP%3EHAL_Delay(10)%3B%3C%2FP%3E%3CP%3Eg_bccConfig.drvInstance%20%3D%200%3B%3C%2FP%3E%3CP%3Eg_bccConfig.commMode%20%3D%20BCC_MODE_TPL%3B%3C%2FP%3E%3CP%3Eg_bccConfig.devicesCnt%20%3D%201%3B%3C%2FP%3E%3CP%3Eg_bccConfig.device%20%3CSPAN%20class%3D%22%22%3E%5B0%5D%3C%2FSPAN%3E%3D%20BCC_DEVICE_MC33771C%3B%3C%2FP%3E%3CP%3Eg_bccConfig.cellCnt%20%3CSPAN%20class%3D%22%22%3E%5B0%5D%3C%2FSPAN%3E%3D%2014%3B%3C%2FP%3E%3CP%3Estatus%20%3D%20BCC_Init(%26amp%3Bg_bccConfig)%3B%3C%2FP%3E%3CP%3Eif(status%20!%3D%20BCC_STATUS_SUCCESS)%3C%2FP%3E%3CP%3E%7B%3C%2FP%3E%3CP%3Ereturn%20(int)status%3B%3C%2FP%3E%3CP%3E%7D%3C%2FP%3E%3CP%3E%7D%3C%2FP%3E%3CP%3Evoid%20HAL_SPI_RxCpltCallback(SPI_HandleTypeDef%20*hspi)%3C%2FP%3E%3CP%3E%7B%3C%2FP%3E%3CP%3Eif(hspi-%26gt%3BInstance%20%3D%3D%20SPI2)%3C%2FP%3E%3CP%3Espi2_rx_done%20%3D%201%3B%3C%2FP%3E%3CP%3E%7D%3C%2FP%3E%3CP%3Estatic%20void%20MX_SPI1_Init(void)%3C%2FP%3E%3CP%3E%7B%3C%2FP%3E%3CP%3Ehspi1.Instance%20%3D%20SPI1%3B%3C%2FP%3E%3CP%3Ehspi1.Init.Mode%20%3D%20SPI_MODE_MASTER%3B%3C%2FP%3E%3CP%3Ehspi1.Init.Direction%20%3D%20SPI_DIRECTION_2LINES%3B%3C%2FP%3E%3CP%3Ehspi1.Init.DataSize%20%3D%20SPI_DATASIZE_8BIT%3B%3C%2FP%3E%3CP%3Ehspi1.Init.CLKPolarity%20%3D%20SPI_POLARITY_LOW%3B%3C%2FP%3E%3CP%3Ehspi1.Init.CLKPhase%20%3D%20SPI_PHASE_2EDGE%3B%3C%2FP%3E%3CP%3Ehspi1.Init.NSS%20%3D%20SPI_NSS_SOFT%3B%3C%2FP%3E%3CP%3Ehspi1.Init.BaudRatePrescaler%20%3D%20SPI_BAUDRATEPRESCALER_8%3B%3C%2FP%3E%3CP%3Ehspi1.Init.FirstBit%20%3D%20SPI_FIRSTBIT_MSB%3B%3C%2FP%3E%3CP%3Ehspi1.Init.TIMode%20%3D%20SPI_TIMODE_DISABLE%3B%3C%2FP%3E%3CP%3Ehspi1.Init.CRCCalculation%20%3D%20SPI_CRCCALCULATION_DISABLE%3B%3C%2FP%3E%3CP%3Ehspi1.Init.NSSPMode%20%3D%20SPI_NSS_PULSE_ENABLE%3B%3C%2FP%3E%3CP%3Eif(HAL_SPI_Init(%26amp%3Bhspi1)%20!%3D%20HAL_OK)%3C%2FP%3E%3CP%3E%7B%3C%2FP%3E%3CP%3E%E3%82%A8%E3%83%A9%E3%83%BC%E3%83%8F%E3%83%B3%E3%83%89%E3%83%A9%E3%83%BC()%3B%3C%2FP%3E%3CP%3E%7D%3C%2FP%3E%3CP%3E%7D%3C%2FP%3E%3CP%3Estatic%20void%20MX_SPI2_Init(void)%3C%2FP%3E%3CP%3E%7B%3C%2FP%3E%3CP%3Ehspi2.Instance%20%3D%20SPI2%3B%3C%2FP%3E%3CP%3Ehspi2.Init.Mode%20%3D%20SPI_MODE_SLAVE%3B%3C%2FP%3E%3CP%3Ehspi2.Init.Direction%20%3D%20SPI_DIRECTION_2LINES_RXONLY%3B%3C%2FP%3E%3CP%3Ehspi2.Init.DataSize%20%3D%20SPI_DATASIZE_8BIT%3B%3C%2FP%3E%3CP%3Ehspi2.Init.CLKPolarity%20%3D%20SPI_POLARITY_LOW%3B%3C%2FP%3E%3CP%3Ehspi2.Init.CLKPhase%20%3D%20SPI_PHASE_2EDGE%3B%3C%2FP%3E%3CP%3Ehspi2.Init.NSS%20%3D%20SPI_NSS_HARD_INPUT%3B%3C%2FP%3E%3CP%3Ehspi2.Init.FirstBit%20%3D%20SPI_FIRSTBIT_MSB%3B%3C%2FP%3E%3CP%3Ehspi2.Init.TIMode%20%3D%20SPI_TIMODE_DISABLE%3B%3C%2FP%3E%3CP%3Ehspi2.Init.CRCCalculation%20%3D%20SPI_CRCCALCULATION_DISABLE%3B%3C%2FP%3E%3CP%3Ehspi2.Init.NSSPMode%20%3D%20SPI_NSS_PULSE_DISABLE%3B%3C%2FP%3E%3CP%3Eif(HAL_SPI_Init(%26amp%3Bhspi2)%20!%3D%20HAL_OK)%3C%2FP%3E%3CP%3E%7B%3C%2FP%3E%3CP%3E%E3%82%A8%E3%83%A9%E3%83%BC%E3%83%8F%E3%83%B3%E3%83%89%E3%83%A9%E3%83%BC()%3B%3C%2FP%3E%3CP%3E%7D%3C%2FP%3E%3CP%3E%7D%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-LABS%20id%3D%22lingo-labs-2369103%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CLINGO-LABEL%3E%E3%83%9C%E3%83%BC%E3%83%89%E8%A8%AD%E8%A8%88%3C%2FLINGO-LABEL%3E%3C%2FLINGO-LABS%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2370557%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%20translate%3D%22no%22%3ERe%3A%20MC33771c%20TPL%20communication%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2370557%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3E%E3%83%9F%E3%83%A9%E3%83%AB%E6%A7%98%E3%80%81%3C%2FP%3E%0A%3CP%3E%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%82%A8%E3%83%B3%E3%82%B8%E3%83%8B%E3%82%A2%E3%81%8B%E3%82%89%E3%81%AE%E5%9B%9E%E7%AD%94%E3%81%AF%E4%BB%A5%E4%B8%8B%E3%81%AE%E3%81%A8%E3%81%8A%E3%82%8A%E3%81%A7%E3%81%99%E3%80%82%E3%81%94%E8%A6%81%E6%9C%9B%E3%81%A9%E3%81%8A%E3%82%8A%E3%80%81%E3%82%B9%E3%82%B3%E3%83%BC%E3%83%97%E3%82%92%E5%85%B1%E6%9C%89%E3%81%97%E3%81%A6%E3%81%8F%E3%81%A0%E3%81%95%E3%81%84%E3%80%82%3C%2FP%3E%0A%3CP%3E%E8%AA%AC%E6%98%8E%3C%2FP%3E%0A%3CP%3E%3CFONT%20color%3D%22%230000FF%22%3E%3CSPAN%3E%E9%A1%A7%E5%AE%A2%E3%81%8C%E9%80%81%E4%BF%A1%E6%99%82%E3%81%AE%E3%82%AA%E3%82%B7%E3%83%AD%E3%82%B9%E3%82%B3%E3%83%BC%E3%83%97%E6%B3%A2%E5%BD%A2%E3%82%84Saleae%E3%81%AE%E5%87%BA%E5%8A%9B%E7%B5%90%E6%9E%9C%E3%82%92%E5%85%A5%E6%89%8B%E3%81%A7%E3%81%8D%E3%82%8C%E3%81%B0%E3%80%81%E4%BD%95%E3%81%8C%E8%B5%B7%E3%81%93%E3%81%A3%E3%81%A6%E3%81%84%E3%82%8B%E3%81%AE%E3%81%8B%E3%82%92%E6%AD%A3%E7%A2%BA%E3%81%AB%E6%8A%8A%E6%8F%A1%E3%81%99%E3%82%8B%E3%81%AE%E3%81%AB%E9%9D%9E%E5%B8%B8%E3%81%AB%E5%BD%B9%E7%AB%8B%E3%81%A1%E3%81%BE%E3%81%99%E3%80%82MC33771B%E3%81%AFTPL1%EF%BC%8840%E3%83%93%E3%83%83%E3%83%88%EF%BC%89%E3%80%81MC33771C%E3%81%AFTPL2%EF%BC%8848%E3%83%93%E3%83%83%E3%83%88%EF%BC%89%E3%81%A7%E3%81%82%E3%82%8B%E3%81%93%E3%81%A8%E3%81%AB%E6%B3%A8%E6%84%8F%E3%81%97%E3%81%A6%E3%81%8F%E3%81%A0%E3%81%95%E3%81%84%E3%80%82%E3%81%BE%E3%81%9F%E3%80%81%E3%81%8A%E5%AE%A2%E6%A7%98%E3%81%AF%E6%B7%BB%E4%BB%98%E3%81%AEMC33771C%20SDK%E3%82%92%E5%8F%82%E7%85%A7%E3%81%99%E3%82%8B%E3%81%93%E3%81%A8%E3%82%82%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%80%82%3C%2FSPAN%3E%3C%2FFONT%3E%3C%2FP%3E%0A%3CP%3E%E6%95%AC%E5%85%B7%E3%80%81%3C%2FP%3E%0A%3CP%3E%E3%83%A8%E3%82%BC%E3%83%95%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2369482%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%20translate%3D%22no%22%3ERe%3A%20MC33771c%20TPL%20communication%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2369482%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3E%3CSPAN%3E%E9%A1%A7%E5%AE%A2%EF%BC%9AAARTRONIX%20INNOVATIONS%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%3E%E6%9C%80%E7%B5%82%E9%A1%A7%E5%AE%A2%EF%BC%9AAAROHI%20EMBEDDED%20SYSTEM%20PVT%20LTD%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%3E%E6%9C%80%E7%B5%82%E7%94%A8%E9%80%94%EF%BC%9AUPS%E3%83%90%E3%83%83%E3%83%86%E3%83%AA%E3%83%BC%E3%83%90%E3%83%83%E3%82%AF%E3%82%A2%E3%83%83%E3%83%97%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%3E%E5%9B%BD%3A%20%E3%82%A4%E3%83%B3%E3%83%89%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%3E%E5%B9%B4%E9%96%93%E7%99%BA%E8%A1%8C%E9%87%8F%EF%BC%9A1000%3C%2FSPAN%3E%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2369464%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%20translate%3D%22no%22%3ERe%3A%20MC33771c%20TPL%20communication%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2369464%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3E%E3%83%9F%E3%83%A9%E3%83%AB%E6%A7%98%E3%80%81%3C%2FP%3E%0A%3CP%3E%E3%81%8A%E5%AE%A2%E6%A7%98%E3%81%AE%E5%95%8F%E9%A1%8C%E3%81%AB%E3%81%A4%E3%81%84%E3%81%A6%E3%80%81%E3%82%BD%E3%83%95%E3%83%88%E3%82%A6%E3%82%A7%E3%82%A2%E3%82%A8%E3%83%B3%E3%82%B8%E3%83%8B%E3%82%A2%E3%81%AB%E9%80%A3%E7%B5%A1%E3%81%99%E3%82%8B%E5%BF%85%E8%A6%81%E3%81%8C%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82%E3%83%97%E3%83%AD%E3%82%B8%E3%82%A7%E3%82%AF%E3%83%88%E3%81%AB%E9%96%A2%E3%81%99%E3%82%8B%E4%BB%A5%E4%B8%8B%E3%81%AE%E6%83%85%E5%A0%B1%E3%82%92%E3%81%8A%E7%9F%A5%E3%82%89%E3%81%9B%E3%81%8F%E3%81%A0%E3%81%95%E3%81%84%E3%80%82%E5%BD%BC%E3%82%89%E3%81%AF%E5%B8%B8%E3%81%AB%E6%83%85%E5%A0%B1%E3%82%92%E5%BF%85%E8%A6%81%E3%81%A8%E3%81%99%E3%82%8B%E3%80%82%3C%2FP%3E%0A%3CP%20class%3D%22x_elementToProof%22%3E%3CFONT%20color%3D%22%230000FF%22%3E%3CSPAN%20data-olk-copy-source%3D%22MessageBody%22%3E%E9%A1%A7%E5%AE%A2%EF%BC%9AAARTRONIX%20INNOVATIONS%3C%2FSPAN%3E%3C%2FFONT%3E%3C%2FP%3E%0A%3CP%20class%3D%22x_elementToProof%22%3E%3CFONT%20color%3D%22%230000FF%22%3E%3CSPAN%3E%E6%9C%80%E7%B5%82%E9%A1%A7%E5%AE%A2%EF%BC%9A%EF%BC%9F%EF%BC%88AARTRONIX%20INNOVATIONS%E3%81%AE%E5%A0%B4%E5%90%88%E3%82%82%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%EF%BC%89%3C%2FSPAN%3E%3C%2FFONT%3E%3C%2FP%3E%0A%3CP%20class%3D%22x_elementToProof%22%3E%3CFONT%20color%3D%22%230000FF%22%3E%3CSPAN%3E%E6%9C%80%E7%B5%82%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%3A%20%3F%3C%2FSPAN%3E%3C%2FFONT%3E%3C%2FP%3E%0A%3CP%20class%3D%22x_elementToProof%22%3E%3CFONT%20color%3D%22%230000FF%22%3E%3CSPAN%3E%E5%9B%BD%3A%20%E3%82%A4%E3%83%B3%E3%83%89%3C%2FSPAN%3E%3C%2FFONT%3E%3C%2FP%3E%0A%3CP%20class%3D%22x_elementToProof%22%3E%3CFONT%20color%3D%22%230000FF%22%3E%3CSPAN%3E%E5%B9%B4%E9%96%93%E8%B2%A9%E5%A3%B2%E9%87%8F%EF%BC%9A%EF%BC%9F%3C%2FSPAN%3E%3C%2FFONT%3E%3C%2FP%3E%0A%3CP%3E%E6%95%AC%E5%85%B7%E3%80%81%3C%2FP%3E%0A%3CP%3E%E3%83%A8%E3%82%BC%E3%83%95%3C%2FP%3E%3C%2FLINGO-BODY%3E