Looking for eIQ command line tool to convert TFlite mode to the NPU of MCXN947

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Looking for eIQ command line tool to convert TFlite mode to the NPU of MCXN947

1,553 Views
ramkumarkoppu_p
Contributor III

Hi,

I remember there is used to be command line converter tool to convert TFlite model to utilise the operators available on the NPU of MCXN947, now couldn't find this tool on the NXP website. can you help to me find and download this command line to use it both Ubuntu 22.04 and apple silicon Mac please?

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

1,511 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @ramkumarkoppu_p 

You can download the eIQ® Toolkit from the below link.

eIQ® Toolkit | NXP Semiconductors

HangZhang_0-1729496609168.png

It includes the MODEL TOOL and COMMAND LINE.

BR

Hang

0 Kudos
Reply