IMX93 Deep Sleep Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX93 Deep Sleep Mode

1,475 Views
dhruvinrajpura
Contributor III

In the A core of IMX93,
As per given in power measurement doc(AN13917) followed steps given in section 6.7.9,

1)Boot the Linux image with imx93-11x11-evk-DSM.dtb.

2) echo mem > /sys/power/state

3) Measure the power and record the results


while measuring power,

vdd_soc is showing 15mA and 9.36mW and GROUP_SOC_FULL is 25mW avg but as per power measurement doc GROUP_SOC_FULL should be 7.56mW.

I want to take GROUP_SOC_FULL as much down as possilble, What I can do to achive GROUP_SOC_FULL as 7.56mW?

 

#imx93 #imx

Labels (2)
0 Kudos
Reply
1 Reply

1,438 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @dhruvinrajpura 

 

Could you please tell me what BSP version are you using? Also, your SOM version.

 

Best regards,

Salas.

0 Kudos
Reply