How to use the npu on mcxn947

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to use the npu on mcxn947

跳至解决方案
913 次查看
TomC818
Contributor III

I would like to try to deploy model beside from the computer visions ones shown from the demo in application hub.
I would like to know how the npu is being declared or used in the demo codes. The demo codes don't seems to directly interact with the npu. Are there any APIs or function to utilize the on-chip npu? Or is the npu automatically managed?

标签 (1)
0 项奖励
回复
1 解答
860 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @TomC818 

You're correct that in the MCXN947 demos, the NPU is not typically accessed through direct API calls in the application code. Instead, the NPU is automatically invoked by the TensorFlow Lite for Microcontrollers runtime.

You can refer to the dm-multiple-person-detection-on-mcxn947 demo.

BR

Harry

在原帖中查看解决方案

1 回复
861 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @TomC818 

You're correct that in the MCXN947 demos, the NPU is not typically accessed through direct API calls in the application code. Instead, the NPU is automatically invoked by the TensorFlow Lite for Microcontrollers runtime.

You can refer to the dm-multiple-person-detection-on-mcxn947 demo.

BR

Harry