How to use LIN on s32g

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use LIN on s32g

1,814 Views
LB666
Contributor I

How to verify the communication function of two LIN channels on the Linux driver of BSP37 when there are two LIN channels on the S32g274A RDB2 development board

 

0 Kudos
Reply
3 Replies

1,777 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @LB666

Thanks for the reply

There are LIN support in RTD SW packages, you may test/modify the examples in it to test the LIN function according to the requirements.

 

Best Regards

Chenyin

0 Kudos
Reply

1,798 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @LB666

Thanks for the question

Seems you want to test the LIN under Linux in BSP37? Well, current Linux BSP releases do not include support for the LIN mode of LinFlexD, only UART mode supported in newer BSP versions.

If you want to verify the LIN functions, we suggest using the drivers available in RTD SW packages.

 

Best Regards

Chenyin

0 Kudos
Reply

1,788 Views
LB666
Contributor I
Okay, so how do I test LLCE-LIN? Can you provide some reference materials
0 Kudos
Reply