How to restore MCU-Link firmware

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to restore MCU-Link firmware

跳至解决方案
916 次查看
Maccha_Neko
Contributor I

I obtained an FRDM board and installed MCUXpresso on a Linux (under VMware....Host OS is Windows11).

When I launched the debugger, there was a firmware update available, so I proceeded with it.

 However, during the USB reconnection, it took a long time, and I encountered an error.

Since then, the FRDM board is recognized as a USB device, but MCU-Link is no longer detected.

Is there any way to recover it?"

标签 (1)
0 项奖励
回复
1 解答
887 次查看
Harry_Zhang
NXP Employee
NXP Employee

HI @Maccha_Neko 

Which chip's FRDM development board are you currently using?

If you want to update your firmware.

1. Download the linkserver software and install it.

Search | NXP Semiconductors

2. Enter the ISP mode.

3. 

Harry_Zhang_0-1744083271511.png

Double click the program_CMSIS.cmd

And press enter.

BR

Harry

在原帖中查看解决方案

0 项奖励
回复
2 回复数
888 次查看
Harry_Zhang
NXP Employee
NXP Employee

HI @Maccha_Neko 

Which chip's FRDM development board are you currently using?

If you want to update your firmware.

1. Download the linkserver software and install it.

Search | NXP Semiconductors

2. Enter the ISP mode.

3. 

Harry_Zhang_0-1744083271511.png

Double click the program_CMSIS.cmd

And press enter.

BR

Harry

0 项奖励
回复
808 次查看
Maccha_Neko
Contributor I

I appologize for the late reply.
I'm using FRDM-MCXN947.
I tried it according to your instructions, it was successful.
The FRDM board works well again.
I appreciate your help.

0 项奖励
回复