How to restore MCU-Link firmware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to restore MCU-Link firmware

Jump to solution
923 Views
Maccha_Neko
Contributor I

I obtained an FRDM board and installed MCUXpresso on a Linux (under VMware....Host OS is Windows11).

When I launched the debugger, there was a firmware update available, so I proceeded with it.

 However, during the USB reconnection, it took a long time, and I encountered an error.

Since then, the FRDM board is recognized as a USB device, but MCU-Link is no longer detected.

Is there any way to recover it?"

Labels (1)
0 Kudos
Reply
1 Solution
894 Views
Harry_Zhang
NXP Employee
NXP Employee

HI @Maccha_Neko 

Which chip's FRDM development board are you currently using?

If you want to update your firmware.

1. Download the linkserver software and install it.

Search | NXP Semiconductors

2. Enter the ISP mode.

3. 

Harry_Zhang_0-1744083271511.png

Double click the program_CMSIS.cmd

And press enter.

BR

Harry

View solution in original post

0 Kudos
Reply
2 Replies
895 Views
Harry_Zhang
NXP Employee
NXP Employee

HI @Maccha_Neko 

Which chip's FRDM development board are you currently using?

If you want to update your firmware.

1. Download the linkserver software and install it.

Search | NXP Semiconductors

2. Enter the ISP mode.

3. 

Harry_Zhang_0-1744083271511.png

Double click the program_CMSIS.cmd

And press enter.

BR

Harry

0 Kudos
Reply
815 Views
Maccha_Neko
Contributor I

I appologize for the late reply.
I'm using FRDM-MCXN947.
I tried it according to your instructions, it was successful.
The FRDM board works well again.
I appreciate your help.

0 Kudos
Reply