How to program flash via UART ISP for MCXC242?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to program flash via UART ISP for MCXC242?

Jump to solution
2,884 Views
limit1995
Contributor II
  1. Is there tool like flashmagic to program flash via UART ISP for MCXC242?  If no, How to?
  2. Does MCUXpresso Sec support MCXC242?  I found there is no MCXC series MCU. limit1995_1-1731404162652.png

     

 

Labels (2)
0 Kudos
Reply
1 Solution
2,799 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi limit1995 

Currently we can use blhost under command line. We are working on the article but it's not availabe yet. For the moment, you can refer to this one. it's for Kinetis but the method is the same.

https://mcuoneclipse.com/2017/07/12/getting-started-rom-bootloader-on-the-nxp-frdm-kl03z-board/

Best Regards,

Jun Zhang

View solution in original post

0 Kudos
Reply
4 Replies
2,874 Views
marek-trmac
NXP Employee
NXP Employee

Hi Limit,

MCUXpresso Secure Provisioning tool does not support MCX C yet. It shall be supported in 2025 (release date not confirmed yet).

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 Kudos
Reply
2,841 Views
limit1995
Contributor II

Hi Marek,

So what could be used to program flash via UART?

 

Tags (1)
0 Kudos
Reply
2,800 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi limit1995 

Currently we can use blhost under command line. We are working on the article but it's not availabe yet. For the moment, you can refer to this one. it's for Kinetis but the method is the same.

https://mcuoneclipse.com/2017/07/12/getting-started-rom-bootloader-on-the-nxp-frdm-kl03z-board/

Best Regards,

Jun Zhang

0 Kudos
Reply
2,756 Views
limit1995
Contributor II
Thanks for your support.
0 Kudos
Reply