Failing to measure bandgap voltage on channel 27

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failing to measure bandgap voltage on channel 27

Jump to solution
1,975 Views
Weber1
Contributor II

Hi community,

I'm using an MCXA156 and continuously failing to get plausible values when reading channel 27 of ADC0, which is the bandgap. All other channels (including temperature measurement on channel 26) work fine.

I tried different configurations of the ADC channel command like different sample time, different numbers of conversion, different resolution modes, but failing to get a plausible value of 1.0V: value/adc_resolution*VDDA-voltage, e.g. value=380, resolution=4096, VDDA-voltage=3.3V -> 0.3V.

Strangely my values differ depending on the configured sample time, (e.g. 5806 @65536 or 14800 @32768 resolution which is opbviously wrong). Of course I read in multiple values which seem to be constant (+noise, maybe more than expected) but nevertheless not showing the expected value of 1.0V. I even went back to the basics and tried it on my demo board FRDM_MCXA156 using the SDK code example "frdmmcxa156_lpadc_interrupt", which also fails to show me the correct bandgap values.

Is there anything special about reading the bandgap from ADC0 like it is for the temperature channel?

Maybe I have to route the bandgap signal to the ADC manually? Couldn't anything like this in the manual/datasheet.

Any other ideas how to solve it?

Regards

Weber

Labels (1)
0 Kudos
Reply
1 Solution
1,343 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Weber1 

Thanks for your patience. 

The bandgap should be enabled before use.

You can use the function SPC_SetActiveModeBandgapModeConfig(SPC0, kSPC_BandgapEnabledBufferEnabled);

Alice_Yang_1-1758620590832.png


It is working fine now.

Alice_Yang_0-1758620589523.png

 

BR

Alice

 

  

 

 

 

View solution in original post

0 Kudos
Reply
8 Replies
1,344 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Weber1 

Thanks for your patience. 

The bandgap should be enabled before use.

You can use the function SPC_SetActiveModeBandgapModeConfig(SPC0, kSPC_BandgapEnabledBufferEnabled);

Alice_Yang_1-1758620590832.png


It is working fine now.

Alice_Yang_0-1758620589523.png

 

BR

Alice

 

  

 

 

 

0 Kudos
Reply
1,337 Views
Weber1
Contributor II

Hi Alice,
this works perfectly fine! Thank you!
Seems to be my fault, which was not obvious to me from the manual. But it's not very obvious, I'd say.

By the way: Any ideas what's the bandgap buffer? (BGMODE=10b - Bandgap enabled, buffer enabled)

Weber1_0-1758624635705.png

BR

Weber

 

0 Kudos
Reply
1,639 Views
Weber1
Contributor II

Hi Alice,

thank you for your efforts. Getting a value of 0 seems also wrong, because expecting 1V of bandgap voltage.

My results are like this:

Weber1_0-1757402610138.png

The HW setup is as simple as it can be: Windows-laptop -> USB -> FRDM-MCXA156 board -> (nothing else connected)

Weber1_1-1757402789201.png

Any further ideas? Maybe anybody else used the bandgap voltage measurement with or without success?

BR
Weber

 

0 Kudos
Reply
1,491 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi @Weber1 

Yes, it’s also incorrect on my side. All zeros even use your project.

Alice_Yang_0-1757649039585.png


I will investigate it deeply and confirm with internal teams.
Sorry for the inconvenience caused.

I’ll keep you updated with any progress.
Thank you.

 

BR

Alice

1,800 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Weber1 

Thanks for your patience.
Are you using the FRDM-MCXA156 board?
Please send your project to me, and I will help test and check it on my side.
Thank you.

 

BR

Alice

0 Kudos
Reply
1,723 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Weber1 

Hope you are well. Just wanted to check back and see if you had a chance to review my previous email. Maybe you've already fixed this problem, else don't hesitate to contact us.

 

BR

Alice

0 Kudos
Reply
1,717 Views
Weber1
Contributor II

Hi,

thank you for the quick reply. Yes, I'm using the FRDM-MCXA156 board and just imported the lpadc_polling example and made a few changes like 

#define DEMO_LPADC_BASE ADC0
#define DEMO_LPADC_USER_CHANNEL 27

With this, I'm getting values around 5900 at high-resolution, which indicates that bandgap voltage is 0.3V.

Find attached the project files.

BR
Weber

Tags (3)
0 Kudos
Reply
1,655 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Weber1 

I have tested your project on my side, but I always get almost 0 every time. I am using the FRDM-MCXA156 board.

Alice_Yang_0-1757323864036.png

Could you please share a photo of your hardware connections, as well as the test results from your side?
Thank you.
 
BR
Alice
 

 

0 Kudos
Reply