FRDM-MCXN947 SD Card Slot Part Number

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-MCXN947 SD Card Slot Part Number

1,966 Views
stevenlutz
Contributor III

I have the FRDM-MCXN947 and want to add the optional SD Card slot that gets soldered to the board. However, I can't seem to find the correct sd card slot that fits the board properly. 
I have checked the guides, docs, BOM etc for the board, and it's no where to be listed that I can see. 
Can someone provide the proper part number that I can easily order from the likes of mouser, or digi-key?

FRDM-MCXN947 

Labels (1)
0 Kudos
Reply
3 Replies

1,920 Views
stevenlutz
Contributor III

Thank you, I couldn't find it in the BOM I downloaded form the site and isn't mentioned in the schematics. 

0 Kudos
Reply

1,916 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @stevenlutz 

 

Please download from the following link : https://www.nxp.com/webapp/Download?colCode=FRDM-MCXN947-DESIGN-FILES 

 

BR

Alice

0 Kudos
Reply

1,937 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @stevenlutz 

According to the BOM, please use MEM2075-00-140-01-A from GLOBAL CONNECTOR TECHNOLOGY INC.


 
Updating Media

 

Best Regards,

Alice

 

0 Kudos
Reply