FRDM-MCXN947 Power Via Pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FRDM-MCXN947 Power Via Pin

跳至解决方案
953 次查看
John_Adams
Contributor I

Hello, I would like to ask, is there a way to power the FRDM-MCXN947 board (with 5V) externally via pin without using USB-C?

 

Thank you very much

John Adams

标签 (3)
0 项奖励
回复
1 解答
891 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @John_Adams 

Yes, you can refer to the FRDM-MCXN947 schematic.

 
 

Snipaste_2025-02-07_11-56-57.png

5V power supply can choose any one of P5V_MCU_LINK_USB, P5V_USB_HS and P5V_HDR_IN.

BR

Harry

在原帖中查看解决方案

0 项奖励
回复
1 回复
892 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @John_Adams 

Yes, you can refer to the FRDM-MCXN947 schematic.

 
 

Snipaste_2025-02-07_11-56-57.png

5V power supply can choose any one of P5V_MCU_LINK_USB, P5V_USB_HS and P5V_HDR_IN.

BR

Harry

0 项奖励
回复