Hello,
in my application on FRDM-MCX947 board that's based on FreeRTOS, I try to detect USB_HS using USB stack. I always have a situation that the first connection after starting the program is not detected by the interrupt (it does not jump to the USB1_HS_IRQHandler) and when disconnecting the USB1_HS_IRQHandler is called, the next connection is also detected, but once in a while it drops out again.
In the main function in the initialization phase, I initialize the USB stack and enable the interrupt:
void APP_UsbInit(void)
{
USB_DeviceClockInit();
g_msc.speed = USB_SPEED_FULL;
g_msc.attach = 0;
g_msc.deviceHandle = NULL;
if (kStatus_USB_Success != USB_DeviceInit(CONTROLLER_ID, USB_DeviceCallback, &g_msc.deviceHandle))
{
usb_echo("USB device mass storage init failed\r\n");
return;
}
SDK_DelayAtLeastUs(5000, SDK_DEVICE_MAXIMUM_CPU_CLOCK_FREQUENCY);
USB_DeviceIsrEnable();
}
void USB_DeviceIsrEnable(void)
{
uint8_t irqNumber;
uint8_t usbDeviceEhciIrq[] = USBHS_IRQS;
irqNumber = usbDeviceEhciIrq[CONTROLLER_ID - kUSB_ControllerEhci0];
/* Install isr, set priority, and enable IRQ. */
DisableIRQ((IRQn_Type)irqNumber);
NVIC_SetPriority((IRQn_Type)irqNumber, USB_DEVICE_INTERRUPT_PRIORITY);
EnableIRQ((IRQn_Type)irqNumber);
}
Then, if a connected USB is detected, I initialize Mass Storage and switch the program to Mass Storage mode using a semaphore, however, it is probably not invoked on the first connection:
void USB1_HS_IRQHandler(void)
{
BaseType_t xHigherPriorityTaskWoken = pdFALSE;
if (false == bMscInitialized)
{
/* Initialize The Mass Storage Device Application */
/* @note Initialization SD Card In Device Mode */
USB_DeviceApplicationInit();
bMscInitialized = true;
}
USB_DeviceEhciIsrFunction(g_msc.deviceHandle);
/* Free The Mutex For Mass Storage Task */
xSemaphoreGiveFromISR(g_TaskMutex, &xHigherPriorityTaskWoken);
/**
* Switch The Context From ISR To a Higher Priority Task,
* Without Waiting For The Next Scheduler Tick.
**/
portYIELD_FROM_ISR(xHigherPriorityTaskWoken);
}
I would like to ask if there is anything else to add during initialization to make my detection work properly. Thank you in advance for all your advice.