FRDM-MCXN947 Cannot download program to chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-MCXN947 Cannot download program to chip

1,333 Views
dreamdf
Contributor I

MCUXpresso IDE RedlinkMulti Driver v24.9 

Reconnected to existing LinkServer process.

Connecting to probe 1 core 0 (using server started externally) reports:

Could not connect to core

图片1.png

I flash my program via kiel a few times.I come across debug abort when i try to

debug.Then I lost my board, series port works well, but cannot flash new project

0 Kudos
Reply
5 Replies

1,303 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @dreamdf 

It seems that your MCU is temporally bricked.

To recover the debug access, please try to set the MCU into ISP mode, this way bootROM will execute, setting the MCU into a known state. Once it is set into this state, please try to do a mass erase and program your application one more time. 

Please let me know your results.

Diego

0 Kudos
Reply

1,236 Views
dreamdf
Contributor I

I use MCUXpresso Secure Provisioning Tool flash a demo successfully.

Program run normally.

But cannot flash KEil project bin file.Program doesnot run.

Still canont download file via keil or MCXpresso IDE

Program MCU-Link CMSIS-DAP - CNXPMCU-LINK_installer cannot updata debugger.

Tags (1)
0 Kudos
Reply

1,089 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @dreamdf 

I am sorry for the delayed respose, I missed your reply.

I understand that you can program over ISP, but did you used USB connection or UART?

Did you manage to find out something else during this time? If yes please let me know. 

Other thing we could check is : jumper setup on your FRDM board, could you share a picture where we can see the jumpers?

 

Diego

 

0 Kudos
Reply

1,275 Views
dreamdf
Contributor I

I downloaded blhost and entry isp mode successfully, I erased flash and downloaded a offical demo.But My Board still doesnot work after resetting.

dreamdf_0-1732954114208.png

 

0 Kudos
Reply

1,292 Views
dreamdf
Contributor I
Hello,How can I set the FRDM-MCXN947 into ISP mode,And what should I do to erase the flashed program.
Sorry for this simple question, I am a Newbie
0 Kudos
Reply