FRDM-MCXC242 Dev Board SPI Slave Select Manual Control

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-MCXC242 Dev Board SPI Slave Select Manual Control

364 Views
sachindia86
Contributor I

Objective : Board to Board SPI Communication 

I am using SDK examples

frdmmcxc242_spi_polling_b2b_transfer_master

frdmmcxc242_spi_polling_b2b_transfer_slave

By default in this examples SPI Slave Select is configured automatic. However my requirement is to do it manually. 

Please provide the SDK examples with manual Slave Select support.

 

#MCX242

#

0 Kudos
Reply
1 Reply

343 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @sachindia86 

You can manually select the slave via a GPIO. It is simple.

Feel free to contact me if still have any issue about it. 

 

BR

Alice

 

BR

Alice

0 Kudos
Reply