Error on LWIP library

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error on LWIP library

5,646 次查看
Faries_Abdullah
Contributor I

I am having an error when compiling my code. This code is from the previous engineer who poorly documented the code. I deleted the debug and release file before I cleaned and built the code on my laptop. I also have to manually include files. After that, I have an error on LWIPlibrary inside where it says error: field 'call' has incomplete type. I check the code and I don't think there is a problem with the library. Could this be the problem with how I compile the code? or the file inclusion? I stuck for two days for this. I use ebf1052 and use mimxrt1052 for MCU.

标签 (3)
0 项奖励
回复
1 回复

5,589 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @Faries_Abdullah 

Can you share your project so that I can easily reproduce this issue?

BR

Hang

0 项奖励
回复