Error on LWIP library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error on LWIP library

6,402件の閲覧回数
Faries_Abdullah
Contributor I

I am having an error when compiling my code. This code is from the previous engineer who poorly documented the code. I deleted the debug and release file before I cleaned and built the code on my laptop. I also have to manually include files. After that, I have an error on LWIPlibrary inside where it says error: field 'call' has incomplete type. I check the code and I don't think there is a problem with the library. Could this be the problem with how I compile the code? or the file inclusion? I stuck for two days for this. I use ebf1052 and use mimxrt1052 for MCU.

ラベル(3)
0 件の賞賛
返信
1 返信

6,345件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @Faries_Abdullah 

Can you share your project so that I can easily reproduce this issue?

BR

Hang

0 件の賞賛
返信