Error on LWIP library

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error on LWIP library

6,617 Views
Faries_Abdullah
Contributor I

I am having an error when compiling my code. This code is from the previous engineer who poorly documented the code. I deleted the debug and release file before I cleaned and built the code on my laptop. I also have to manually include files. After that, I have an error on LWIPlibrary inside where it says error: field 'call' has incomplete type. I check the code and I don't think there is a problem with the library. Could this be the problem with how I compile the code? or the file inclusion? I stuck for two days for this. I use ebf1052 and use mimxrt1052 for MCU.

Labels (3)
0 Kudos
Reply
1 Reply

6,560 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @Faries_Abdullah 

Can you share your project so that I can easily reproduce this issue?

BR

Hang

0 Kudos
Reply