EIQ validation winerror 10048

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EIQ validation winerror 10048

2,163件の閲覧回数
Jasmine_zzz
Contributor I

After training a model with EIQtoolkit, I intended to perform PTQ and validate it on the test set, but I encountered the error shown in the picture. I've tried restarting my computer multiple times and reinstalling the software, yet the problem persists. Now I've got no idea what to do.

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,134件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello,

Would you please share the screenshot of the error you are seeing?

Regards,
Gustavo

0 件の賞賛
返信

2,111件の閲覧回数
Jasmine_zzz
Contributor I

Sorry to bother but I just encountered another error as is shown below. I tried to deploy the model and it seemed to be wrong with the device. But I got no idea how to deal with this problem.

屏幕截图 2025-05-07 113535.png屏幕截图 2025-05-07 113535.png

 

屏幕截图 2025-05-07 113817.png屏幕截图 2025-05-07 113817.png

 

0 件の賞賛
返信

2,118件の閲覧回数
Jasmine_zzz
Contributor I

I'm really sorry. The image failed to upload when I made the post. Here is the error screenshot.

I've tried several times and got error messages shown in the two pictures. 

屏幕截图 2025-05-05 220042.png屏幕截图 2025-05-05 220042.png

 

屏幕截图 2025-05-06 095321.png屏幕截图 2025-05-06 095321.png

0 件の賞賛
返信

2,067件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @Jasmine_zzz 

Based on your screenshot, it seems to be a network issue. Can you try using a different network again?

BR

Harry

0 件の賞賛
返信