16bit differential adc config

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

16bit differential adc config

1,264 次查看
Dirk3
Contributor I

I want to use the 16bit differential ADC on the FRDM MCXN947 dev board. I cannot get the configuration correct. See the screenshots attached to see the configuration in Config Tools. My main code is added as code sample, could someone help me figure out why I cannot get a result from the ADC. 

/*
 * Copyright 2016-2024 NXP
 * All rights reserved.
 *
 * SPDX-License-Identifier: BSD-3-Clause
 */

/**
 * @file    ADC_test4.c
 * @brief   Application entry point.
 */
#include <stdio.h>
#include "board.h"
#include "peripherals.h"
#include "pin_mux.h"
#include "clock_config.h"
#include "MCXN947_cm33_core0.h"
#include "fsl_debug_console.h"
#include "fsl_lpadc.h"
#include "fsl_ctimer.h"
#include "fsl_spc.h"

/*******************************************************************************
 * Variables
 ******************************************************************************/
volatile uint32_t adcResult = 0U;
volatile bool g_LpadcConversionCompletedFlag = false;
lpadc_conv_result_t convResult;

/*******************************************************************************
 * Definitions
 ******************************************************************************/

/* ADC IRQ handler */
void ADC0_IRQHandler(void) {
    PRINTF("ADC0 interrupt triggered\n");
    #if (defined(FSL_FEATURE_LPADC_FIFO_COUNT) && (FSL_FEATURE_LPADC_FIFO_COUNT == 2U))
        if (LPADC_GetConvResult(ADC0, &convResult, 0U))
    #else
        if (LPADC_GetConvResult(ADC0, &convResult))
    #endif /* FSL_FEATURE_LPADC_FIFO_COUNT */
    {
        g_LpadcConversionCompletedFlag = true;
    }
    SDK_ISR_EXIT_BARRIER;
}



/*!
 * @brief Main function
 */
int main(void) {

    /* Init board hardware. */
    SPC_EnableActiveModeAnalogModules(SPC0, kSPC_controlVref);
    BOARD_InitBootPins();
    BOARD_InitBootClocks();
    BOARD_InitBootPeripherals();
    BOARD_InitDebugConsole();


    /* Enable interrupts for ADC0 */
    LPADC_EnableInterrupts(ADC0, kLPADC_Trigger0CompletionInterruptEnable | kLPADC_FIFO0WatermarkInterruptEnable);
    EnableIRQ(ADC0_IRQn);

    PRINTF("Please input any character to get the ADC result\r\n");
    while (1) {

        GETCHAR();
        LPADC_DoSoftwareTrigger(ADC0, 1U);
        while(!g_LpadcConversionCompletedFlag) {
        }
        PRINTF("ADC Result: %d\n", convResult.convValue);
        g_LpadcConversionCompletedFlag = false;
    
        }

    return 0;
}

Dirk3_0-1716381764699.pngDirk3_1-1716381781776.png

Dirk3_2-1716381805379.png

 

0 项奖励
回复
1 回复

1,207 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Dirk3 

Please check below settings.

1> Use oscilloscope confirm there is input signal in ADC channel of your board.

2>Config ADC input pin correctly.

3>Enabled clock.

4>Using ADC demo under SDK to test firstly, whether can work without any issue?

 

BR

Alice

0 项奖励
回复