eIQ Neutron NPU Lab Guides

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

eIQ Neutron NPU Lab Guides

eIQ Neutron NPU Lab Guides

These lab guides provide step-by-step instructions on how to take a quantized TensorFlow Lite model and use the Neutron Conversion Tool found in eIQ Neutron SDK to convert the model to run on the eIQ Neutron NPU found on NXP MCU devices. 

The eIQ Neutron NPU for MCX N Lab Guide  documents focus on using the Neutron Converter tool found inside eIQ Neutron SDK to convert a model and then import that converted model into an eIQ MCUXpresso SDK example. There are labs for VSCode, GCC, and MCUXpresso IDE.


The labs designed to run on the FRDM-MCXN947 but the same concepts can be applied to other MCX N boards as well. There is a similar NPU lab available for i.MX RT700 too. 

Also be sure to also check out the Getting Started community post for more details on the eIQ Neutron NPU.

---
Updated January 2026 for eIQ Neutron SDK and MCUXpresso SDK 25.12. The Neutron Converter tool was previously included in eIQ Toolkit but is now released as part of the new eIQ Neutron SDK. 

标签 (2)
附件
100% 有帮助 (2/2)
版本历史
最后更新:
昨天
更新人: