How to update the debugger of the MCX - N & MCX - A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to update the debugger of the MCX - N & MCX - A

How to update the debugger of the MCX - N & MCX - A

FRDM-MCXA153

FRDM-MCXA153.png

FRDM-MCXN947 

FRDM-MCXN947.png

 

Hardware & Software

To do this, surely you have to download the next software.

About the hardware.

MCU Link Firmware update.

We will need the firmware to update the LPC55s69 on the board, the MCU Link firmware version 2.263 is compatible with the MCX.

You may need the EVK connected to the computer under DFU mode, in the schematic of the EVK does not mention the DFU but has the named jumper of ISP [JP21] MCX - N or [JP8] MCX - A, sure you put the LPC55s69 in ISP, not the MCX, review the schematic below.

MCX - N

Pavel_Hernandez_2-1705689983333.png

MCX - A

Pavel_Hernandez_3-1705689994953.png

When you have installed this version on your computer, go to the locations.

ROOT: C:\nxp\MCU-LINK_installer_2.263\scripts

Pavel_Hernandez_4-1705690003136.png
Then open the CMD prompt console and run the script for CMSIS.
Pavel_Hernandez_5-1705690057711.png

The console asks if you have the appropriate jumper, if yes click enter again.

Pavel_Hernandez_6-1705690072853.png

If everything is right the message successfully will appear.

Pavel_Hernandez_7-1705690087444.png

Then in the MCUXpresso, you can see the debugger probe.

Pavel_Hernandez_8-1705690099720.png

Happy Debugging.

ラベル(3)
評価なし
バージョン履歴
最終更新日:
‎01-22-2024 03:35 PM
更新者: