Enabling Hardware Trigger-Based ADC Input Sampling for PWM Duty Cycle Control-with FRDM-MCXA156

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Enabling Hardware Trigger-Based ADC Input Sampling for PWM Duty Cycle Control-with FRDM-MCXA156

Enabling Hardware Trigger-Based ADC Input Sampling for PWM Duty Cycle Control-with FRDM-MCXA156

This document introduces how to configure and use the hardware trigger feature of the Analog-to-Digital Converter (ADC) on the FRDM-MCXA156 development board.

It presents an event where using an external button initiates a reading and ADC conversion that reads an analog input from a potentiometer; the resulting digital value is then used to dynamically update the duty cycle of a PWM signal connected to an external output represented by a LED.

This example demonstrates the usage of external connections and analog measurement by walking through the modifications required to enable hardware triggering via the Input Multiplexing (INPUTMUX) module.

附件
无评分
版本历史
最后更新:
2 周之前
更新人: