Enabling Hardware Trigger-Based ADC Input Sampling for PWM Duty Cycle Control-with FRDM-MCXA156

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enabling Hardware Trigger-Based ADC Input Sampling for PWM Duty Cycle Control-with FRDM-MCXA156

Enabling Hardware Trigger-Based ADC Input Sampling for PWM Duty Cycle Control-with FRDM-MCXA156

This document introduces how to configure and use the hardware trigger feature of the Analog-to-Digital Converter (ADC) on the FRDM-MCXA156 development board.

It presents an event where using an external button initiates a reading and ADC conversion that reads an analog input from a potentiometer; the resulting digital value is then used to dynamically update the duty cycle of a PWM signal connected to an external output represented by a LED.

This example demonstrates the usage of external connections and analog measurement by walking through the modifications required to enable hardware triggering via the Input Multiplexing (INPUTMUX) module.

添付
評価なし
バージョン履歴
最終更新日:
‎08-28-2026 02:33 PM
更新者: