MCUXpresso VS Code Import Repository Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso VS Code Import Repository Error

Jump to solution
11,476 Views
jagararno
Contributor II

I'm trying to port an MCUXpresso Eclipse project to Visual Studio Code.
I followed all the instructions on the web site
For 'Location' I create an empty folder "C:\User\james\git\mcu_file"
For 'Repository' I select "MCUXpresso SDK"
Then all the files are cloned and everything looks good, but I get this message in the 'OUTPUT' console:
[error] C
ould not read settings from mcuxpresso-tools.json for project "c:\Users\james\git"
I appreciate any guidance you can provide. Thanks!

 

0 Kudos
Reply
1 Solution
11,273 Views
jagararno
Contributor II

Thanks for your help, Christian.

I've decided to continue with the Eclipse-based MCUXpresso until January, then I'll try again.

View solution in original post

0 Kudos
Reply
6 Replies
11,438 Views
DragosMiloiu
NXP Employee
NXP Employee

Hi @jagararno,

After the conversion is complete, if you go to "c:\Users\james\git\.vscode", do you have a mcuxpresso-tools.json file? If you do, could you please attach it here?

Thanks,

Dragos.

 

0 Kudos
Reply
11,436 Views
jagararno
Contributor II

The only file in C:\Users\james\git\.vscode is settings.json, which contains a single entry:

{
"git.ignoreLimitWarning": true
}

 

0 Kudos
Reply
11,431 Views
DragosMiloiu
NXP Employee
NXP Employee

Could you please try to convert the project again from MCUXpresso IDE to VS Code and see if there is any error/warning logged in MCUXpresso for VS Code console after the conversion?

DragosMiloiu_0-1693491526061.png

Thanks,

Dragos.

0 Kudos
Reply
11,407 Views
jagararno
Contributor II

Thank you for looking into this problem.

I have attached the entire "Import Project" sequence with the OUTPUT content.

0 Kudos
Reply
11,372 Views
cristiantepus
NXP Employee
NXP Employee

Hi,

It is possible to generate a simple project in MCUXpresso IDE that produces this conversion error and you can send us to reproduce? or some instructions how to generate such a project that generates the error on conversion?

If none of the above possible:

- what NXP device is the project intended for?

- is this project an MCUXpresso IDE managed project, having linker files generated by IDE (so not a pure makefile project type but a project that was originally created using the MCUXpresso wizard/importer)? 

- is this linked to an MCUXpresso SDK? which one (its name, including version)?

- do you use in your project files that are not on your current disk (i.e. remote locations, another drive, ...)?

- is it a single project or it has some other linked projects (example: multicore, trustzone, linked library, ...)?

Regards,

Cristian

0 Kudos
Reply
11,274 Views
jagararno
Contributor II

Thanks for your help, Christian.

I've decided to continue with the Eclipse-based MCUXpresso until January, then I'll try again.

0 Kudos
Reply