LPC5536: LPCXpresso55S36 Development Board supported?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC5536: LPCXpresso55S36 Development Board supported?

Jump to solution
1,849 Views
danielholala
Senior Contributor II

Hello,

I'm using MCUXpresso for VS Code for the first time. 

I started by installing a repository, i.e., the MCUXpresso SDK from github.

Then I wanted to import an example from this repository but the LPCXpresso55S36 Development Board seems not supported, see screenshot:

danielholala_0-1695740954451.png

That's strange, as the MCUXpresso SDK clearly contains files for the LPC5536 processor, see here:

https://github.com/nxp-mcuxpresso/mcux-sdk/tree/main/devices/LPC5536

Please advise!

Thanks.
Daniel

 

 

0 Kudos
Reply
1 Solution
1,802 Views
Xu_Zhang
NXP Employee
NXP Employee

Hi, danielholala

When I set up the repository, the version I chose was MCUX_2.14.0_LPC55S36. I can find the LPCXpresso55S36 Development Board.

Xu_Zhang_0-1695798408635.png

Xu_Zhang_1-1695798432201.png

There is another way you can try, You can download the LPCXpresso55S36 Development Board from MCUXpresso SDK Builder, download address for https://mcuxpresso.nxp.com/en/welcome, Note the following Toolchain options, select ALL Toolchain.

Xu_Zhang_0-1695783654737.png

Download the sdk in the C:\VS_Code\ SDK_2_14_0_LPCXpresso55S36.zip directory and install a repository locally.


 
Updating Media

 


Then, import the LPCXpresso55S36 development board sample.

Xu_Zhang_2-1695783691329.png

 

BR

Xu Zhang

 

View solution in original post

5 Replies
1,803 Views
Xu_Zhang
NXP Employee
NXP Employee

Hi, danielholala

When I set up the repository, the version I chose was MCUX_2.14.0_LPC55S36. I can find the LPCXpresso55S36 Development Board.

Xu_Zhang_0-1695798408635.png

Xu_Zhang_1-1695798432201.png

There is another way you can try, You can download the LPCXpresso55S36 Development Board from MCUXpresso SDK Builder, download address for https://mcuxpresso.nxp.com/en/welcome, Note the following Toolchain options, select ALL Toolchain.

Xu_Zhang_0-1695783654737.png

Download the sdk in the C:\VS_Code\ SDK_2_14_0_LPCXpresso55S36.zip directory and install a repository locally.


 
Updating Media

 


Then, import the LPCXpresso55S36 development board sample.

Xu_Zhang_2-1695783691329.png

 

BR

Xu Zhang

 

1,792 Views
danielholala
Senior Contributor II

Dear @Xu_Zhang ,

Thank you for your support. Somehow I missed the "MCUX_2.14.0_LPC55S36" entry. Following your instructions, I installed this version of the MCUXpresso SDK and now I can select the "LPCXpresso LPC55S36 board" when importing an example.

Note that I ordered the LPC5536-EVK which, obviously, hosts a LPC5536 and not a LPC55S36.

I tried the "led_blinky" example and now see that the device is set to "LPC55S36". Should that bother me?

See screenshot:

danielholala_0-1695802612708.png

Have a nice day.
Daniel

0 Kudos
Reply
1,759 Views
Xu_Zhang
NXP Employee
NXP Employee

hi,danielholala

When building the sdk, you can try to select the following figure.

image.png

 

BR

Xu Zhang

0 Kudos
Reply
1,729 Views
danielholala
Senior Contributor II

Hello Xu Zhang,

I tried it with a standalone SDK generated and downloaded from SDK Builder.

That does not change anything:

danielholala_0-1695979427816.png

 

The examples are the same. They are depending on the board that I select and there are only LPC55S36-based boards selectable.

danielholala_1-1695979524139.png

 

0 Kudos
Reply
1,586 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @danielholala 

There is no problem, just use it.

 

BR

Alice

0 Kudos
Reply