Hi, is there a guide for how to connect the IMXRT1160 EVK with the secure provisioning tool (V8) as I'm getting connection failed when trying to use the USB port. I've tried both USB1 & USB2 on the EVK but get the same result. Also does a specific example program need to be run when trying to connect?
Any suggestions greatly appreciated.
Kind regards
Ian
Solved! Go to Solution.
Hi Ian,
1. check the power supply, J38 should be set to 3-4 for power from USB
2. check the switches to set the board to ISP mode: SW1: 0001 (to run the application, change the switch to 0010)
Here is the photo of RT1170-EVK, where the jumpers are located and where the cable should be connected. RT1160-EVK should be similar.
Hi Ian,
1. check the power supply, J38 should be set to 3-4 for power from USB
2. check the switches to set the board to ISP mode: SW1: 0001 (to run the application, change the switch to 0010)
Here is the photo of RT1170-EVK, where the jumpers are located and where the cable should be connected. RT1160-EVK should be similar.