MCUXpresso Secure Provisioning tool Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso Secure Provisioning tool Problem

ソリューションへジャンプ
3,057件の閲覧回数
Seongyon_Jeong
Contributor III

I’m currently working with the RT1020-EVK board, connected to my PC via USB cable.
I’ve configured the board’s boot mode to BOOT_MODE[1:0] = 01 for Serial Downloader Mode.

However, in this configuration, the board fails to connect over USB, and only UART communication works correctly

Seongyon_Jeong_0-1750927771585.png

. 

Seongyon_Jeong_1-1750927863341.png

 

Could you please advise why this might be happening?
Also, if I want to use the USB interface with Serial Downloader Mode, are there any additional steps or configurations I should apply?

Thank you for your support.



0 件の賞賛
返信
1 解決策
3,024件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hi Seongyon,

 

regarding the DIP switches I cannot provide any feedback.

Regarding USB vs UART - what USB port do you use? 

If I am correct:

J9 - this should be used for USB ISP 

J23 - for UART ISP

 

you also need to check you power supply, if you do not use external one, see `MIMXRT1020 EVK Board Hardware User’s Guide`

liborukropec_0-1751016717480.png

 

Regards,

Libor

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,044件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hi,

 

in addition what Marek wrote - do you see the EVK in the device manager?

Also please note, that ROM is sticky to a channel that it can see at first, so if you started communicating via UART, to try the USB you have to reset the chip so the ROM again looks for the both UART and USB and which is the first, it will stick to it again.

 

And see the PDF for the EVK, frequently the different USB port has to be used for UART and another one for USB and even power supply source has to be changed via jumpers based on the used USB port.

 

Regards,

Libor

0 件の賞賛
返信
3,052件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi,

the board should be switched to ISP mode.

You can find the DIP SWITCH configuration in the user guide - processor specific workflow

Processor-specific workflows — MCUXpresso Secure Provisioning Tool 25.03 25.03 documentation

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 件の賞賛
返信
3,031件の閲覧回数
Seongyon_Jeong
Contributor III

I already  switched  ISP mode.

Table DIP Switches: Boot mode selection for EVKs
Seongyon_Jeong_0-1750984944677.png


My EVK  board dip switch.

Seongyon_Jeong_1-1750985061906.png

This may be a bit off-topic, but I would like to raise a hardware-related concern.

I frequently need to change the DIP switch settings—specifically switches 3 and 4—for XIP boot configuration. However, I’ve found that the DIP switches are quite small and feel somewhat fragile. After repeated use, I’m concerned they may be getting damaged or worn out.

Would it be possible to consider using larger and more robust DIP switches in future revisions of the board?

0 件の賞賛
返信
3,025件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hi Seongyon,

 

regarding the DIP switches I cannot provide any feedback.

Regarding USB vs UART - what USB port do you use? 

If I am correct:

J9 - this should be used for USB ISP 

J23 - for UART ISP

 

you also need to check you power supply, if you do not use external one, see `MIMXRT1020 EVK Board Hardware User’s Guide`

liborukropec_0-1751016717480.png

 

Regards,

Libor

0 件の賞賛
返信
2,990件の閲覧回数
Seongyon_Jeong
Contributor III
Now I understand why this occured .
Thanks for your reply. !
0 件の賞賛
返信