MCUXpresso Secure Provisioning Tool Encrypt settings area

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso Secure Provisioning Tool Encrypt settings area

1,368件の閲覧回数
tobias91
Contributor III

Hi,

trying out MCUXpresso Secure Provisioning Tool with  LPC55S28 chip. Was able to add the bootloader binary and with the "additional images"  options add the application. But also want to add an area where settings will be written when the device is runnng and be saved encrypted. Is there a way to do this?

 

Br

Tobias

0 件の賞賛
返信
1 返信

1,303件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi Tobias,

as additional image, you can add any binary content you need, including data files and binary blobs.

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 件の賞賛
返信