MCUXpresso Secure Provisioning Tool Encrypt settings area

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso Secure Provisioning Tool Encrypt settings area

578 Views
tobias91
Contributor III

Hi,

trying out MCUXpresso Secure Provisioning Tool with  LPC55S28 chip. Was able to add the bootloader binary and with the "additional images"  options add the application. But also want to add an area where settings will be written when the device is runnng and be saved encrypted. Is there a way to do this?

 

Br

Tobias

0 Kudos
Reply
1 Reply

512 Views
marek-trmac
NXP Employee
NXP Employee

Hi Tobias,

as additional image, you can add any binary content you need, including data files and binary blobs.

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 Kudos
Reply