MCUXpresso Secure Provisioning TOOL issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCUXpresso Secure Provisioning TOOL issue

1,982 次查看
Maheshkadam9922
Contributor II

I have led blinky .bin file , here we use J flash tool to flash the bin file at address 0x60000000 and its working ok 

but same .bin file I tried to flash using secure provisioning tool- tool - flash programmer at x60000000  but its not working

 

0 项奖励
回复
1 回复

1,974 次查看
marek-trmac
NXP Employee
NXP Employee

Hi Mahesh,

can you share your SEC tool workspace? From description you provided it is hard to guess, where the problem is. We even do not know what processor are you using.

Can you write the image using JFlash and verify it in flash programmer? You should see the differences.

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 项奖励
回复