MCUXpresso Secure Provisioning TOOL issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso Secure Provisioning TOOL issue

1,986件の閲覧回数
Maheshkadam9922
Contributor II

I have led blinky .bin file , here we use J flash tool to flash the bin file at address 0x60000000 and its working ok 

but same .bin file I tried to flash using secure provisioning tool- tool - flash programmer at x60000000  but its not working

 

0 件の賞賛
返信
1 返信

1,978件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi Mahesh,

can you share your SEC tool workspace? From description you provided it is hard to guess, where the problem is. We even do not know what processor are you using.

Can you write the image using JFlash and verify it in flash programmer? You should see the differences.

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 件の賞賛
返信