unable to build for fusion F1 DSP MIMXRT595-EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

unable to build for fusion F1 DSP MIMXRT595-EVK

379件の閲覧回数
Nicolas-ph
Contributor II
Hi,
 
When trying to build one of the examples (following https://mcuxpresso.nxp.com/mcuxsdk/25.06.00/html/boards/RT/evkmimxrt595/gettingStartedXplorer/topics...) I get the following error:
[nicolas@LPC84-nicolas xcc]$ make
[  5%] Building C object CMakeFiles/dsp_naturedsp_dsp.elf.dir/opt/mcuxpresso-ide/SDK_25_06_00_EVK-MIMXRT595/SDK_25_06_00_EVK-MIMXRT595/boards/evkmimxrt595/dsp_examples/naturedsp/fusionf1/main.c.obj
Error: the "nxp_rt500_RI23_11_newlib" core is not in the current Xtensa core registry.

You need to either specify the name of a registered Xtensa core (with
the --xtensa-core option or the XTENSA_CORE environment variable) or
specify a different registry of Xtensa cores (with the --xtensa-system
option or the XTENSA_SYSTEM environment variable).

The following Xtensa cores are available:
<None>
 
The  is set to XTENSA_SYSTEM is set .../builds/RI-2023.11-linux/nxp_rt500_RI23_11_newlib. XTENSA_CORE is set to "nxp_rt500_RI23_11_newlib", but is not found. No cores are available?
 
When using the Xplorer application I get the same error. The DSP configuration for linux newlib was downloaded from tensilica tools and installed using the GUI.
The specific build error is: 
**** Incremental Build [Wed, 23 Jul 2025 11:46:42] ****
 Project: test
 Configuration: nxp_rt500_RI23_11_newlib
 Build Target: Debug
********************************
....

LLVM ERROR: Failed to load library ~/xtensa/XtDevTools/install/builds/RI-2023.11-linux/nxp_rt500_RI23_11_newlib/config/llvm/lib/libXtensaCodeGen.so. Unsupported processor configuration. ~/xtensa/XtDevTools/install/builds/RI-2023.11-linux/nxp_rt500_RI23_11_newlib/config/llvm/lib/libXtensaCodeGen.so: cannot enable executable stack as shared object requires: Invalid argument

....
 
 
Could there be something wrong with the DSP configuration for linux (newlib) v10.1.11 download from tenisillica tools? Is anyone else experiencing issues on Linux?
 
0 件の賞賛
返信
4 返答(返信)

250件の閲覧回数
Nicolas-ph
Contributor II

Hi Gavin,

Thank you for the reply. 

If the license is not ok, I am unable to start the build process in the IDE. So that should not be it. Also, the Xplorer IDE reports that the license is ok in both windows and Linux.

Best regards,
Nicolas

0 件の賞賛
返信

201件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @Nicolas-ph ,

I did the same test for you on a test environment and the problem should be in the environment variable configuration. Modify it to the following configuration and it will work:

XTENSA_SYSTEM=~/xtensa/XtDevTools/install/builds/RI-2023.11-linux/nxp_rt500_RI23_11_newlib/config
export XTENSA_CORE=nxp_rt500_RI23_11_newlib export 

Gavin_Jia_0-1754990046173.png

 

Best regards,
Gavin

0 件の賞賛
返信

375件の閲覧回数
Nicolas-ph
Contributor II
Update, going through the same steps on windows, I am able to build...
0 件の賞賛
返信

256件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @Nicolas-ph ,

Thanks for your interest in NXP MIMXRT series!

The Windows environment can compile DSP code, so your configuration process should be fine. I just suspect that it could be due to a problem with the license in a Linux environment.

Gavin_Jia_0-1754468219833.png

 

Best regards,
Gavin

0 件の賞賛
返信