share SDK builder configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

share SDK builder configuration

2,468 Views
grzegorzkonopko
Contributor III

Hi

I am working in team under single project. SDK configuration is build via web page, download on disk and import to MCUXpresso.

How I can ensure that everyone in team use exactly the same version of build? Is a way of sharing this configuration or build ?

REgards

/GReg

5 Replies

2,229 Views
PetrKraus
NXP Employee
NXP Employee

Hi GReg,

In order to ensure that someone gets the exactly same SDK configuration as you have, you can share a link to your SDK configuration with that person. Click the share action icon on your SDK entry on the MCUXpresso website dashboard page to get the link.

Regards,

Petr

2,229 Views
grzegorzkonopko
Contributor III

Hi Petr

I am looking "share" icon, but can not find, could you attach screenshot?

Regards

/Greg

0 Kudos
Reply

2,229 Views
grzegorzkonopko
Contributor III

Hi

No such icon on my dashboard..

pastedImage_3.png

0 Kudos
Reply

2,229 Views
PetrKraus
NXP Employee
NXP Employee

Hi Greg,

pastedImage_1.png

0 Kudos
Reply

2,229 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello GReg,

How about using version control ,  for example git ,  have a look at the below threads:

How to manage MCUXpresso SDK versions in git?  

How do two or more developers work on the same project ?  

Hope it helps,


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply