sdmmc eMMC Decode CID properly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

sdmmc eMMC Decode CID properly

5,092件の閲覧回数
JohnU
Contributor III

Hi,

Patch proposal for SDK 2.2.0 (LPCXpresso54608):

Date:   Fri Jun 30 13:37:31 2017 +0200

    sdmmc: fix MMC_DecodeCid() according to MMC spec (not SD spec)

    JSED84-B45 and Physical Layer Simplified Specification Version 2.00
    define a little different CID fields structure.

diff --git a/sdmmc/src/fsl_mmc.c b/sdmmc/src/fsl_mmc.c
index e980aa4..770930d 100755
--- a/sdmmc/src/fsl_mmc.c
+++ b/sdmmc/src/fsl_mmc.c
@@ -1497,13 +1497,14 @@ static void MMC_DecodeCid(mmc_card_t *card, uint32_t *rawCid)
     cid->productName[2U] = (uint8_t)((rawCid[2U] & 0xFF0000U) >> 16U);
     cid->productName[3U] = (uint8_t)((rawCid[2U] & 0xFF00U) >> 8U);
     cid->productName[4U] = (uint8_t)((rawCid[2U] & 0xFFU));
+    cid->productName[5U] = (uint8_t)((rawCid[1U] & 0xFF000000U) >> 24U);

-    cid->productVersion = (uint8_t)((rawCid[1U] & 0xFF000000U) >> 24U);
+    cid->productVersion = (uint8_t)((rawCid[1U] & 0xFF0000U) >> 16U);

-    cid->productSerialNumber = (uint32_t)((rawCid[1U] & 0xFFFFFFU) << 8U);
-    cid->productSerialNumber |= (uint32_t)((rawCid[0U] & 0xFF000000U) >> 24U);
+    cid->productSerialNumber = (uint32_t)((rawCid[1U] & 0xFFFFU) << 16U);
+    cid->productSerialNumber |= (uint32_t)((rawCid[0U] & 0xFFFF0000U) >> 16U);

-    cid->manufacturerData = (uint16_t)((rawCid[0U] & 0xFFF00U) >> 8U);
+    cid->manufacturerData = (uint16_t)((rawCid[0U] & 0xFF00U) >> 8U);
 }

 static status_t MMC_AllSendCid(mmc_card_t *card)

best regards

J.

タグ(1)
0 件の賞賛
返信
2 返答(返信)

3,942件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

 Is this thread related to the below threads?

sdmmc SD_Write()/SD_Read() failed with ATP card 

https://community.nxp.com/thread/454708 

Regards

Soledad

0 件の賞賛
返信

3,941件の閲覧回数
JohnU
Contributor III

Hi,

no, each of the issues is separate.

The patch concerns MMC chip and the links concerns different SD cards (different initialization problems).

Common things are only library name (sdmmc) and SDIF hardware.

best regards

J.

0 件の賞賛
返信